5/18/2010 11:14 AM | |
Posts: 37 Rating: (2) |
Hi am have to read some data from a gas analyser thruogh modbus communication. The parameters are, Band rate -- 9600 Parity ------- None Stop bits ----- 1 Data lenth ---- 8 bytes the plc configuration is CPU - IM151-8 PN/DP (6ES7-151-8AB00-0AB0) + 1SI module - 6ES7-138-4DF11-0AB0 i found som sample projects but those are with CPU + ET200S + 1SI am not sure that, weather my configuration wil work ???? the same library blocks can be used or not??? thanks in advance AttachmentSI_Modul_via_CP_LIB_v10.zip (293 Downloads) |
Follow us on