8/26/2017 5:43 PM | |
Joined: 9/2/2014 Last visit: 3/18/2024 Posts: 10 Rating: (1) |
Hi, I was studying the Mobus sample project zXX21_04_PtP_Com_MODMA\Modbus Master available in STEP7 Simatic Manager . I came across this surprise cross reference list ( Menu Reference Data / Cross references) to Input bit : I0.0 , Output bit : Q0.0 Memory bit : M0.0 in the Siemens Protected FB7 P_RCV_RK. (Please refer to page#2 of 2 in the attached pdf of the print out of the cross reference list highlighting this.) I think it is a bug. Can some expert confirm it ,please ?. It shakes my confidence if it is really using these bits in the Proetected FBs and the user is unaware of this. From a Beginner Kamath RL ------------------------------------------------------------------------------------------ AttachmentReference data_ zXX21_04_PtP_Co.pdf (48 Downloads) |
Last edited by: Kamath RL at: 8/26/2017 5:44:13 PMLast edited by: The Helping Hand at: 8/29/2017 9:01:34 AMNew subject after splitting |
|
Follow us on