1/27/2017 11:32 AM | |
Posts: 17 Rating: (0) |
[...] My next task is to make a modbus RTU application in C/C++ over one of the serial ports of the iot2040. Is the libmodbus available or must I create it from source? Regards Per ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 1/30/2017 1:00:47 PMNew subject after splitting Last edited by: Min_Moderator at: 1/30/2017 1:02:43 PM |
|
6/27/2017 11:07 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4770 Rating: (123) |
New question published by cri2017 is split to a separate thread with the subject Modbus RTU, high cpu load. Best regards |
Follow us on