9/30/2017 7:37 PM | |
Joined: 2/16/2017 Last visit: 10/17/2024 Posts: 9 Rating: (5) |
Dear TIBI68, Thank you for the great blocks! I was able to implement it in two of our machines.
I was able to integrate it in projects made, both, in Step7 and TIA Portal 13. After migrating and copying your blocks, I only had to select the library version for P_SEND and everything worked like a charm. Thanks again and have a good day! Cheers, Wojtek |
This contribution was helpful to1 thankful Users |
2/14/2018 7:15 AM | |
Joined: 7/16/2008 Last visit: 4/18/2024 Posts: 17 Rating: (0) |
Hello I have a problem with my program for communication with Modbus Slave using MBMAREQ function. Sometimes (one per couple days or weeks) program stops because of Programming Error (Incorrect DB number: 16385). It is trying to acces to block number that I do not use. After that I have to Clear/Reset (from HW Config) and perform Warm Reset, then PLC is working again for some time. Power down/up doesn't helps, the same as only "Warm Reset", I always have to clear memory first and than reset. I'm stuck, don't know how to deal it. Do somebody have some idea? There is 2 last events from diagnostics: Event 1 of 100: Event ID 16# 4562 STOP caused by programming error (OB not loaded or not possible, or no FRB) Breakpoint in user program: Cyclic program (OB1) Priority class: 1 FB number: 10 Module address: 338 Previous operating mode: RUN Requested operating mode: STOP (internal) Internal error, Incoming event 08:28:58.820 2018-02-12 (Coding: 16# 4562 FF84 8E70 0101 000A 0152) Event 2 of 100: Event ID 16# 2532 Block number error when opening a DB Incorrect DB number: 16385 Requested OB: Programming error OB (OB121) OB not found, or disabled, or cannot be started in the in the current operating mode Internal error, Incoming event 08:28:58.810 2018-02-12 (Coding: 16# 2532 FE79 007A 4001 0000 0000) I also attach my project. Thanks in advance goblin AttachmentEnergias.zip (650 Downloads) |
Last edited by: Jen_Moderator at: 2/14/2018 12:13:14 PMNew subject after splitting Last edited by: Jen_Moderator at: 2/15/2018 9:44:47 AMRemoved splitting remark. |
|
2/16/2018 7:23 PM | |
Joined: 7/16/2008 Last visit: 4/18/2024 Posts: 17 Rating: (0) |
I've change the LINK address (MW10->MW100) and I'll see if that helps but it take a couple of days. I also attach corrected project, TIBI68 - can you try to reopen it? Thanks goblin AttachmentEnergias.zip (660 Downloads) |
2/23/2018 12:57 PM | |
Joined: 7/16/2008 Last visit: 4/18/2024 Posts: 17 Rating: (0) |
Today it happened again. Still the same diagnostics errors: Event 1 of 100: Event ID 16# 4562 STOP caused by programming error (OB not loaded or not possible, or no FRB) Breakpoint in user program: Cyclic program (OB1) Priority class: 1 FB number: 10 Module address: 338 Previous operating mode: RUN Requested operating mode: STOP (internal) Internal error, Incoming event 08:28:53.531 2018-02-23 (Coding: 16# 4562 FF84 8E70 0101 000A 0152) Event 2 of 100: Event ID 16# 2532 Block number error when opening a DB Incorrect DB number: 16385 Requested OB: Programming error OB (OB121) OB not found, or disabled, or cannot be started in the in the current operating mode Internal error, Incoming event 08:28:53.521 2018-02-23 (Coding: 16# 2532 FE79 007A 4001 0000 0000) When I went to HW CFG/PLC/Operating Mode and perform "Warm Restart" program has run again. I attach files from Stack dumps when CP was in STOP mode. TIBI68 can you take a look at it? I'll be gratefull for your help. thanks goblin AttachmentStack.zip (639 Downloads) |
Follow us on