6/13/2010 3:54 PM | |
Joined: 2/6/2009 Last visit: 8/19/2024 Posts: 939 Rating: (118) |
Dear All, Attached is the sample project for the Modbus communication between CP341, CP 340 and 1Si (Master) and the third party (slave) devices. Manual for slave devices used in program backup also integrated in the attachment. Main driver block is FB50 (Modbus standard block) andthis block should be called for each master module. Blocks associated with the FB50 is, FB 7 = Modbus_Rcv (Siemens standard block) FB 8 = Modbus_Send (Siemens Standard Block) DB1 = Send list DB (Modbus Queries list) DB3 = Modbus Misc DB4 = Modbus Data (Received Data’s) Advantages of using this block,
Use the Modbus block and achive communication tasks quickly and easily without any problem. Please revert back for any clarification. AttachmentMODBUS_V6.0.zip (4361 Downloads) |
Last edited by: Saravana kumar at: 6/19/2014 1:49 PMLast edited by: Saravana kumar at: 9/14/2013 9:28 AMLast edited by: Saravana kumar at: 8/22/2013 1:41 PMLast edited by: Saravana kumar at: 6/24/2013 12:25 PMPlease download the Attachment from the recent thread Last edited by: Saravana kumar at: 6/24/2013 12:20 PMLast edited by: Saravana kumar at: 6/24/2013 12:19 PMHi, Uploaded is the updated version of Modbus Sample project V5.0. The current backup contains Program for Modbus modules CP 341, CP 340 and 1SI as Modbus masters with a standard slave devices. ************************************************************************************************** Version V5.0 //**Program for CP341 with sample program for Enercon EM6400 Meter //**Program for CP 340 with sample program for Enercon EM6400 Meter //**Program for 1SI with sample program for AREVA Ai205 Meter Last edited by: Saravana kumar at: 4/20/2015 7:00:41 AMLast edited by: Saravana kumar at: 9/23/2015 8:45:53 AMVersion V6.0 Modbus Block WIthout Block Privacy //*Program for CP341 & CP 340 with sample Logic for Enercon EM6400 Meter //*Program for 1SI with sample Logic for AREVA Ai205 Meter Last edited by: Saravana kumar at: 9/23/2015 10:26:24 AMLast edited by: Saravana kumar at: 12/6/2016 6:31:08 AM_______________________________________________________________ |
|
This contribution was helpful to27 thankful Users |
6/14/2010 1:05 PM | |
Posts: 262 Rating: (45) |
thanks buddy it is really helpful... Just like to share that know a days we are insisiting client to go for SIEMENS PAC devices.. i.e. 3100, 3200 & 4200.... instead of EM of conzerve. PAC 3200 has ethernet port inbuilt through which we actually by pass DCS and almost all the wiring and programming ... for details refer the below link :- https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=en&objid=7KM21111BA003AA0&caller=view make full use of it and recommend the same form the our product basket |
Follow us on