1/11/2008 3:45 PM | |
Joined: 8/29/2007 Last visit: 6/9/2022 Posts: 28 Rating: (1) |
Has anyone know some good program (freeware) to simulate MODBUS Master on PC ?? |
1/11/2008 3:49 PM | |
Posts: 16 Rating: (2) |
The kepware OPC Server covers a vast array of protocols. Very useful for testing comms links. http://www.kepware.com/ |
1/12/2008 3:46 PM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating: (318)
|
Hi Pete, 795$ is not freeware I think.... Hi Wachman, I have found a freeware Modbus RTU Serial / Modbus RTU over Ethernet \ Modbus TCP over Ethernet Simulator for test purposes tool. QuickMod Modbus scanning tool I didn't test it because I don't have a Modbus slave here, I have placed the desription of the program in the attachement, you may download it from the link above, it is20Mb. AttachmentQuickMod Modbus scanning tool.pdf (491 Downloads) |
Last edited by: Late at: 12.01.2008 16:01I installed the option runtime only, it started well after sometime installing, I choose the option "QuickMod - Modbus scanner" I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on