2/10/2010 4:50 PM | |
Posts: 5822 Rating: (412)
|
Dear Yogendra, well... these are all parameters of the OUC Open User Communication function... also maybe better known as T-Communication. |
This contribution was helpful to1 thankful Users |
2/10/2010 9:19 PM | |
Joined: 10/3/2008 Last visit: 8/28/2024 Posts: 961 Rating: (124) |
Hi, I don't understand your questions.The answers you can find in the manualand you copied the answerinto your thread already. Have a look at the example project. Here you can see the correct parameterization. Client Simulation: http://www.simplymodbus.ca/ |
This contribution was helpful to1 thankful Users |
2/11/2010 5:36 AM | |
Joined: 11/9/2008 Last visit: 10/4/2024 Posts: 410 Rating: (6) |
Dear Bell & Wuestenraeuber, Thanks For Your Support. I have understand all parameter and i able to establish communication between Modbus Simulator and PLC. I have some problem. I have configure my PLC as Modbus Server and Modbus Simulator act as Client.I able to establish communication between Modbus Simulator and PLC but not able to read or write the data in PLC and Vice versa. May be some parameter gets wrong so please help me to solve this proble. I'm using Holding registor Function Code 03 for data transfer. Please see the attachment of status connection PPT for your refrance. Regards, Yogendra G AttachmentStaus Connection.zip (667 Downloads) |
Last edited by: YogendraG at: 2/11/2010 2:48 PM |
|
2/12/2010 5:01 AM | |
Joined: 11/9/2008 Last visit: 10/4/2024 Posts: 410 Rating: (6) |
[ Dear Bell & Wuestenraeuber, Thanks For Your Support. I have understand all parameter and i able to establish communication between Modbus Simulator and PLC. I have some problem. I have configure my PLC as Modbus Server and Modbus Simulator act as Client.I able to establish communication between Modbus Simulator and PLC but not able to read or write the data in PLC and Vice versa. May be some parameter gets wrong so please help me to solve this proble. I'm using Holding registor Function Code 03 for data transfer. Please see the attachment of status connection PPT for your refrance. Regards, Yogendra G AttachmentStaus Connection.zip (738 Downloads) |
2/15/2010 5:08 AM | |
Joined: 11/9/2008 Last visit: 10/4/2024 Posts: 410 Rating: (6) |
Dear Wuestenraeuber Thanks for support i'm able to communicate. Regards, Yogendra G |
10/26/2010 9:47 PM | |
Posts: 1 Rating: (0) |
Try mosbus reader from www.kurysoft.com |
11/1/2010 10:07 AM | |
Posts: 1 Rating: (0) |
Hi YogendraG I have got the same problem how did you get it fixed |
Follow us on