4/18/2019 12:01 PM | |
Posts: 3 Rating: (1) |
Model Predictive Control on Power Plants! I recently have developed a Model Predictive Control (MPC) for a cement customer. The model was prepared for Kiln & Precalciner when it was made live with the control system, it was able to self control and regulate the plant operation and control on its own without operator's intervention. I am now exploring how to build a Model Predictive Control (MPC) solution for a Power Plant. I need to know the model is built for which area and component/equipment? Please if anyone can help me in this. #MPC #ModelPredictiveControl #APC ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 4/20/2019 10:25:17 AMNew subject after splitting |
|
4/20/2019 10:30 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
Closed cause question posted twice. The second thread with the subject Model predictive control - Which model is built for which area and component/equipment? is published within the conference SIMATIC S7 general. Best regards Jen_Moderator |
This contribution was helpful to1 thankful Users |
Follow us on