3/22/2018 7:12 PM | |
Posts: 80 Rating: (2) |
@bergmanu Great! Infinite Thanks! |
This contribution was helpful to1 thankful Users |
9/17/2018 11:57 AM | |
Joined: 11/17/2016 Last visit: 1/26/2021 Posts: 11 Rating: (1) |
Dear Bergmanu, I followed your described procedure exactly and included openembedded-core-rocko layer into bblayers.conf containing recipes-multimedia with alsa packages inside, specifically "alsa-lib", "alsa-tools", and "alsa-utils" which I added to iot2000-example-image.inc. Then I manually started bitbake process BUT this led to following error messages: ----------------------------- ERROR: iot2000-example-image-1.0-r0 do_rootfs: Unable to install packages. Command '/home/vitus/Dokumente/meta-iot2000/meta-iot2000-example/build/tmp/work/iot2000-poky-linux/iot2000-example-image/1.0-r0/recipe-sysroot-native/usr/bin/opkg --volatile-cache -f /home/vitus/Dokumente/meta-iot2000/meta-iot2000-example/build/tmp/work/iot2000-poky-linux/iot2000-example-image/1.0-r0/opkg.conf -t /home/vitus/Dokumente/meta-iot2000/meta-iot2000-example/build/tmp/work/iot2000-poky-linux/iot2000-example-image/1.0-r0/temp/ipktemp/ -o /home/vitus/Dokumente/meta-iot2000/meta-iot2000-example/build/tmp/work/iot2000-poky-linux/iot2000-example-image/1.0-r0/rootfs --force_postinstall --prefer-arch-to-version install alsa-lib alsa-tools alsa-utils cmake connman connman-client connman-tests connman-tools cronie curl dmidecode dosfstools e2fsprogs galileo-target i2c-tools imageversionfile iot2000setup iptables iw kernel-modules linux-firmware-common minicom modules-load-entries mosquitto mosquitto-clients libmraa-utils nano node-libmraa node-red node-red-contrib-boolean-logic node-red-dashboard node-red-node-intel-gpio node-red-node-serialport nodejs nodejs-npm ofono ofono-tests openssh opkg packagegroup-core-boot packagegroup-core-eclipse-debug packagegroup-core-sdk packagegroup-core-standalone-sdk-target parted pciutils ppp ppp-oe python3-lxml python3-modules python3-pip python3-setuptools run-postinsts screen setledcolor sqlite3 switchmode tree tzcode tzdata tzdata-africa tzdata-americas tzdata-antarctica tzdata-arctic tzdata-asia tzdata-atlantic tzdata-australia tzdata-europe tzdata-misc tzdata-pacific tzdata-posix tzdata-right upm usb-modeswitch usb-modeswitch-data wireless-tools wpa-supplicant' returned 255: Collected errors: * opkg_prepare_url_for_install: Couldn't find anything to satisfy 'alsa-lib'. ERROR: iot2000-example-image-1.0-r0 do_rootfs: Function failed: do_rootfs ERROR: Logfile of failure stored in: /home/vitus/Dokumente/meta-iot2000/meta-iot2000-example/build/tmp/work/iot2000-poky-linux/iot2000-example-image/1.0-r0/temp/log.do_rootfs.25657 ERROR: Task (/home/vitus/Dokumente/meta-iot2000/meta-iot2000-example/recipes-core/images/iot2000-example-image.bb:do_rootfs) failed with exit code '1' ----------------------- which in detail you can see in the attached pdf with sreenshots. I am using latest Ubuntu version on a notebook with native Linux running on it. Would you have any helpful hint for me how to solve this problem? I am really lost here as I try to achieve having "alsa" inside my IoT2040 customized image which by the way is standard in the image for Intel Galileo Gen2 or even Edison. I would appreciate any helpful advice in here. Please help me out. AttachmentError Message.pdf (357 Downloads) |
9/17/2018 12:24 PM | |
Joined: 11/17/2016 Last visit: 1/26/2021 Posts: 11 Rating: (1) |
...here is the metioned log file given in the previous posted and according error message
Attachmentrun.do_rootfs.6058.txt (332 Downloads) |
9/18/2018 11:02 AM | |
Joined: 12/12/2016 Last visit: 4/8/2024 Posts: 640 Rating: (60)
|
Hello, try inserting just alsa-utils inside iot2000-example-image.inc. It will automatically fetch the required dependencies. Also, take notice that only these distros are sanity tested. So you might encounter other errors. Kind regards! |
Follow us on