3/2/2021 1:58 AM | |
Posts: 16 Rating: (0) |
btw can i force/modifying M91.3 & Q6.7? |
Last edited by: Febryn135 at: 03/02/2021 02:00:19 |
|
3/2/2021 2:07 AM | |
Posts: 16 Rating: (0) |
for this program, could we modify value in the address M91.3 & Q6.7? |
3/2/2021 5:30 AM | |
Joined: 9/1/2017 Last visit: 5/19/2024 Posts: 156 Rating: (19) |
Hi
Your project is written in simatic step7 v5.5 And you want to use tia portal v13 and v14? Try to migrate a STEP 7 V5.x project to STEP 7 Professional (TIA Portal) , of course you need step7 v5.x to migrate. Make sure you have secure backup and proceed with another copy. Regards Hosein |
Last edited by: hosein8419 at: 03/02/2021 05:46:43Last edited by: Jen_Moderator at: 03/02/2021 06:39:30Optimized link. |
|
3/2/2021 5:53 AM | |
Joined: 3/30/2020 Last visit: 5/24/2024 Posts: 4533 Rating: (946) |
@Hosein: Good health to you. I do not agree with you. Going to TIA just because Step7 V5.5 is unfamiliar, is not the answer. I see in this topic already two people who are making helpful suggestions in keeping with Step7 V5.5. Changing from Step7 Classic to TIA may have other consequences. The idea is to change as little as possible when troubleshooting / testing. @Febryn: Good day. Have a look at the document that Towome suggested. Chapter 20.8. This will work to force the output. I would not recommend this as it can cause problems if you are not aware of what you will influence. Writing a value to M91.3 is problematic.. regardless which version of Step7 you use. Manipulating the bit in VAT will write the value only once. There after the bit will be modified back to what you show in the program. Making program changes as part of trouble shooting is acceptable for some cases.. as has been said before in this topic. ~ |
Last edited by: qwazee at: 03/02/2021 05:56:40Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
This contribution was helpful to1 thankful Users |
3/2/2021 6:55 AM | |
Posts: 16 Rating: (0) |
so there's no ways to keep value M91.3 hold on its position, right? |
3/2/2021 9:12 AM | |
Joined: 9/1/2017 Last visit: 5/19/2024 Posts: 156 Rating: (19) |
Hi dear qwazee
Thanks for valuable hint, Is it possibl to force plc ( which programmed with step7 v5.5) via tia portal? Ive not done such thing before. Best regards Hosein |
Follow us on