Industry Online Support
Technical Forum
6/10/2013 11:20 AM | |
Posts: 28 Rating: (5) |
Hi everyone, recently i work on project with PLC Siemens S7-300 CPU312C and need to implement PID control. FB41 did well but i read that there is library Modular PID Control which contain more complex function but not included in stdlibrary. Can I use it for CPU312C since this manual not mention anything about CPU312C ? have anyone experienced use it for CPU312C ? best regards, Shaumi Arif Al Faizin |
6/11/2013 7:24 AM | |
Joined: 4/24/2009 Last visit: 8/20/2024 Posts: 2682 Rating: (135) |
Thread closed, because question is published in the following thread,too. Modular PID Control for CPU312C Best regards O_Moderator |
Follow us on