Industry Online Support
Technical Forum
12/4/2012 1:18 PM | |
Posts: 2 Rating: (0) |
Hello, Im using CPU 417-4, and dp/DP coupler 6ES7 158-0ad01-0xa0, gsd file: si01807.gse. After all necessailry things (hw configuration, plug-in, ...) its not working. Ive check everything, connection, BUS, I/O, changing cables, (lenght, other), other DP/DP coupler tested, all working in other project, or testing PLC. In this project are used same dp/dp couplers, with the same configuration and they are working, only this one. Maybe bad gsd file? On the second side is CPU3.. Can anybody help me with this please. Please see the attachment. Thanks for advice
AttachmentERROR.zip (232 Downloads) |
Last edited by: viktor.hric at: 12/4/2012 2:43 PM |
|
This contribution was helpful to3 thankful Users |
Follow us on