8/6/2020 6:01 PM | |
Posts: 8 Rating: (0) |
Hi all Recently I implemented a DP / AS-i Link with PCS7 v8.1 SP1 + APL with AS-Interface PCS 7 Library V8.1 Everything was working very well, but a message appeared in one of the modules on the AS-i network (attached image). Check the CFC and everything is in order, the value is sent for the analog output, when monitoring the hardware it is seen that the value is written, but at the AS-i level the value is not received and consequently there is no current in the output of the module (attached images). I already force the output of the module from the AS-i master and it works correctly, I think that the value is not written in the addresses of that module, because even when changing to the second output it works. I heard that this is a bug in the PCS7 version and is fixed with a HotFix update, but I'm not sure which, nor would I want to implement any. Please if anyone knows which update version is correct or how to solve this, I would greatly appreciate it.
AttachmentAsiError.zip (358 Downloads) |
1/1/2023 3:38 AM | |
Joined: 9/9/2015 Last visit: 4/11/2024 Posts: 727 Rating: (268) |
Hi White, I faced a similar issue, but in AI module. Below is my troubleshooting step for AI card. Troubleshoot steps 1. Check 2 wire / 4 wire configuration, matching with the front connector terminal connection. For 2 wires configuration, ensure terminal 10 and 11 is connected. For 4 wires, ensure it is not. 2. Remove all the field wires, check status 3. power cycle the IO module, check status 4. remove front connector, and reconnect, check status 5. remove front connector, remove module, wait for 5 seconds, reinstall the module and front connector, check status. 6. replace a new moudule , check status. Solution: Step 5 resolved our issue. See this link for similar post. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
This contribution was helpful to1 thankful Users |
Follow us on