3/18/2010 1:08 PM | |
Posts: 5 Rating: (0) |
Hi everybody Order No./ Description Component Version Rack: 0
Order No./ Description Component Version DP master system: 1
AttachmentHW-Config.pdf (567 Downloads) |
This contribution was helpful to1 thankful Users |
3/22/2010 1:19 AM | |
Posts: 16 Rating: (1) |
Hello remember that you are using a fail safe module. i think the problem is wiht the load conected to the ouput. (please see the chart). if you can install a ouput interface relay i think will be the solution. i would like to knoe if you can make the change bye Attachments7300_failsafe_signal_modules_manual_en-US_en-US[1].pdf (1753 Downloads) |
Last edited by: JullioC at: 3/22/2010 1:54 AMTotal correction |
|
8/31/2014 11:19 PM | |
Joined: 9/1/2005 Last visit: 10/14/2024 Posts: 4109 Rating: (195) |
new question published by Uppiis split to a seperate thread with the subject profibus fail of 300 ms 2 times a day. Best regards CS Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on