Industry Online Support
Technical Forum
6/14/2010 3:20 PM | |
Posts: 107 Rating:
|
Hi, I have two module FM541 ( 6ES7451-3AL00-0AE0 ) Thes module are burnt out ( I check some IC inside are burnt ) Please help me to get info, if I replace these two module with new spares, I have to make setting or configure the software again ? or just put the spares and machine can run again ? I need this info because the quotation when I want to order these 2 card module, the supplier said about "INCLUDED" CONFIG. PACKAGE ON cd, what does it means ? Regards, INDRA Attachmentfm541.zip (125 Downloads) |
Follow us on