2/16/2010 8:25 PM | |
Joined: 3/27/2006 Last visit: 10/11/2024 Posts: 90 Rating:
|
This is a pretty impressive suite of tools for providing diagnostic information on an HMI. Unfortunately that's all its for. There is no symbol information in the block. If I want to determine if a station is active in the PLC program it looks like I'll have to use the HMI tags and reverse-engineer a way to do it. Not saying it can't be done, but... All I want to know is if an inverter is actively communicating. |
Last edited by: Blue Moderator at: 16.02.2010 21:58splitted and renamed "I never let a cowboy make the coffee." |
|
2/16/2010 10:02 PM | |
Joined: 10/3/2008 Last visit: 2/14/2025 Posts: 972 Rating:
|
Hi Mojo, If you are interested on another one, have a look at this: www.siemens.com/systemdiagnostics => DP/PA Profibus Slave Diagnostics and Profinet Diagnostics. Wüstenräuber |
Follow us on