Industry Online Support
Technical Forum
5/4/2012 3:33 PM | |
Joined: 3/18/2008 Last visit: 12/8/2023 Posts: 1750 Rating:
|
Here is a link to download PST. i don't know the latest version but you can use it to configure the Scalance Switches. Off Topic. You can also use Simatic Manager for Configuring IP Address for Scalance Switch. Just Connect the Ehternet Cable. Open SimaticManager. Go to PLC and Select Edit Ethernet Node Option. Browse the MAC Address of Device and Configure IP Address and Device name. |
Last edited by: Amit_86 at: 5/4/2012 3:38 PMOFF TOPIC VANDE MATARAM..... |
|
This contribution was helpful to
1 thankful Users |
5/7/2012 8:01 AM | |
Posts: 2 Rating:
|
Actually we use this tool to configure a Scalance W744 ethernet client module. We have both PST V3.2 and V4.0. V3.2 is fine, but does not run on Windows versions higher than Windows XP. Version 4.0 does work with Windows Vista. What we need is a version that is fully compatible with Windows 7 because we don't have Vista and XP is becoming more and more obsolete. I have found that V4 has issues with Windows 7 so that's not an option. I do know a version V4.1 exists for Win7, but I also read that with the release of this version it is no longer a free download. That's why I'm trying to fugure out where I can find version 4.1 of the PST... |
5/7/2012 1:27 PM | |
Joined: 3/18/2008 Last visit: 12/8/2023 Posts: 1750 Rating:
|
Hello mvdh, You can create Support Request for further details on latest Version. Generally We use Simatic Manager V5.5 installed on Windows 7 for configuring the Sclance Swtiches whenever is required. you can find procedure for Simatic Manager in my above reply. Hope this helps. |
VANDE MATARAM..... |
|
5/7/2012 1:41 PM | |
Posts: 139 Rating:
|
Dont forget that the Primary Setup Tool is also normally supplied with the Scalance unit on disc. |
5/7/2012 6:43 PM | |
Posts: 947 Rating:
|
PST is cost-free utlity. and you can install it on any notebook. |
5/7/2012 7:01 PM | |
Posts: 133 Rating:
|
Thanks this was usefull. |
5/10/2012 11:21 AM | |
Joined: 4/24/2006 Last visit: 7/12/2024 Posts: 8711 Rating:
|
Hello, Please have a look at this link: New Primary Setup Tool (PST) version 4.1 and new version V3.2 or 4.0 for address setting of SIMATIC NET Industrial Ethernet products available for download Best regards, Wizard |
Follow us on