10/11/2016 12:34 PM | |
Joined: 9/18/2015 Last visit: 6/4/2024 Posts: 132 Rating: (0) |
|
Last edited by: narove at: 10/11/2016 12:52:51 PM |
|
10/11/2016 12:47 PM | |
Joined: 9/18/2015 Last visit: 6/4/2024 Posts: 132 Rating: (0) |
this is the content of the telegramme used to exchange commande and status data between CU320 and the motor module |
10/11/2016 12:58 PM | |
Joined: 9/18/2015 Last visit: 6/4/2024 Posts: 132 Rating: (0) |
this is the HWconfig |
10/11/2016 1:07 PM | |
Joined: 5/12/2006 Last visit: 8/30/2024 Posts: 22348 Rating: (3006)
|
and what would you tell use with this screens? |
This contribution was helpful to1 thankful Users |
10/11/2016 1:20 PM | |
Joined: 9/18/2015 Last visit: 6/4/2024 Posts: 132 Rating: (0) |
this the function used in SIMOTION CPU code ,which bring data from the telegrammes (between CU320 and motor drive)and send them to I/O data area(between SIMOTION cpu and S7-400 CPU) in I device mode , can anyone help me to interpret it? AttachmentIO_FUNC.txt.zip (239 Downloads) |
Follow us on