Industry Online Support
Technical Forum
7/8/2008 5:12 PM | |
Posts: 31 Rating: (0) |
Dear Sparcky, It depends on the state of the motor, it can be damage in the motor or just tunning for the parameters of themotor. but as I said it depends on the state of the motor which must be seen for diagnose. Hope this help Thanks so much for your participation, Danial. Email: auto_man2k@yahoo.com |
7/11/2008 2:17 PM | |
Posts: 6 Rating: (0) |
Thanks for the reply. We adjusted the following parameters and this resolved the situation; MD1251LOAD_SMOOTH_TIME MD1522ACT_SPEED_FILTER_TIME |
7/21/2008 11:24 PM | |
Posts: 159 Rating: (1) |
You da man! |
Follow us on