4/16/2008 9:08 AM | |
Joined: 5/8/2006 Last visit: 4/29/2024 Posts: 1085 Rating: (77) |
Hi, if you want a moveable window or faceplate during the runtime you can only use the animations "Movement". Single objects can movedwith a script during the runtime, too. I think biggest problem is to move the object by using the mouse. You need the mouse position and you can get the mouse position onlywith an ActiveX element. And there is next problem because you can only use ActiveX elements in a WinCC flexiblePC Runtime. You can read that in the following FAQ (No. 4): http://support.automation.siemens.com/WW/view/de/26165877 Bye |
1/16/2012 3:51 PM | |
Posts: 3037 Rating: (192)
|
Hello, You can find in the following FAQ an example for dynamic positioning of faceplates. See this document "Documentation for dynamic positioning and multiple addressed blocks". Application Example Blocks for STEP 7 and WinCC flexible Tweety |
1/18/2012 10:11 AM | |
Joined: 2/6/2009 Last visit: 5/7/2024 Posts: 938 Rating: (118) |
Hi, The Application example gives the information about the dynamic positioning through script only. I want to know about the Movement of the Faceplate with the cursor aslike Picture window in the WinCC.
|
_______________________________________________________________ |
|
1/18/2012 12:58 PM | |
Posts: 3037 Rating: (192)
|
Yes, that is the posibility which you canuse withstandard function of WinCC flexible. Tweety |
1/18/2012 1:01 PM | |
Posts: 3037 Rating: (192)
|
Hello,
This is not posible with standard functions in WinCC flexible. You can create an own Active X object, which this makes. Here you can find infomations for ActiveX objects. How do you register an ActiveX object on the configuration computer and then incorporate it in WinCC flexible? http://support.automation.siemens.com/WW/view/en/37022154 Is there a Siemens contact for customer-specific software solutions, extensions to WinCC flexible or own applications for Windows CE Panels? http://support.automation.siemens.com/WW/view/en/15247601 Tweety |
Last edited by: Tweety at: 1/18/2012 1:06 PMLast edited by: Tweety at: 1/18/2012 1:04 PM |
|
Follow us on