7/30/2024 12:41 PM | |
Joined: 8/3/2009 Last visit: 9/10/2024 Posts: 13632 Rating:
|
Hello chetjov Moving all the segments to the common archive is not a good idea because these segments will be connected additionally to the taglogging segments and if you have many of them this will decreese the system performance. If the project is basically identical (with only a few changes) you can exchange the RT Data like this: https://support.industry.siemens.com/cs/ww/en/view/24193864 Bye Murof |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
1 thankful Users |
8/1/2024 2:29 PM | |
Joined: 7/15/2019 Last visit: 8/21/2024 Posts: 2 Rating:
|
Hello Murof, thank you very much. It looks like it works. I'll give it a proper test tomorrow. Thank you. |
Follow us on