11/6/2012 1:21 PM | |
Posts: 3037 Rating:
|
Hello walter_g, you can have a look in the following link. How can you transfer a WinCC (TIA Portal) configuration to an operator panel using MPI/PROFIBUS? Do you have integrate your project? See the point 4.2. Tweety |
11/7/2012 1:57 PM | |
Posts: 3037 Rating:
|
Hello walter_g, Do can see your panel and your plc in the "PC/PG interface"? Check the settings of your PLC in TIA Portal under connection. Do you have the right settings of your PLC? Which connectors and cables do I need to connect an OP/PG to an S7 controller? Is there a standard cable? more information SIMATIC NET PROFIBUS Networks Tweety |
11/8/2012 1:24 AM | |
Joined: 7/5/2006 Last visit: 5/19/2023 Posts: 166 Rating:
|
hi Tweety, i reply at your questions: Do can see your panel and your plc in the "PC/PG interface"? with PC adapter is not possible to see them, but i can transfer the project to PLC and to TP1200 Check the settings of your PLC in TIA Portal under connection. see attachment Do you have the right settings of your PLC? see attachment Which connectors and cables do I need to connect an OP/PG to an S7 controller? Is there a standard cable? The cable that i use is the MPI cable of the PG720 more information SIMATIC NET PROFIBUS Networks thanks for your interesting Walter Attachmentproblema_tp1200.pdf (321 Downloads) |
Follow us on