10/12/2011 3:19 PM | |
Joined: 9/11/2011 Last visit: 9/10/2024 Posts: 53 Rating:
|
I want to connect a PC RUNTIME that contains a comunication processor CP 5611 A2 with S7 315 2DP. I joined the WinCC flexible project with the project created by STEP7 but I could not cofiguration the computer for NETPROto be connected to thePLC using the MPI network. How I can do it. Attachmentreseau.zip (74 Downloads) |
10/12/2011 3:37 PM | |
Joined: 3/21/2006 Last visit: 3/30/2025 Posts: 10239 Rating:
|
Hello, Take a look at http://support.automation.siemens.com/WW/view/en/22319131 Best regards, Hristo Mihalev |
10/12/2011 3:57 PM | |
Joined: 9/11/2011 Last visit: 9/10/2024 Posts: 53 Rating:
|
Essayez avec cette orthographe : Merci pour la réponse mais j'ai besoin de la méthode qui permet Saisissez du texte, l'adresse d'un site Web ou importez un document à traduire. Traduction (français > anglais)Thank you for the answer but I need the method that used to configure the processor comunication to get a small red squares in the box named SIMATIC HMI Station. Attachment1.zip (69 Downloads) |
10/12/2011 5:01 PM | |
Joined: 9/11/2011 Last visit: 9/10/2024 Posts: 53 Rating:
|
I have already integrated the WinCC Flex project in Step7 but I did not have the MPI interface in the box of HMI. |
10/12/2011 10:07 PM | |
Joined: 9/11/2011 Last visit: 9/10/2024 Posts: 53 Rating:
|
Thank you I have solved the problem.
AttachmentEXEMPLE.zip (87 Downloads) |
This contribution was helpful to
2 thankful Users |
Follow us on