2/6/2008 7:35 PM | |
Posts: 2661 Rating: (279) |
For GD communication between CPU's in different projectsin a multiproject, essentially there are3 steps: |
2/7/2008 11:50 PM | |
Posts: 2661 Rating: (279) |
Were you able to merge the MPI networks? See attachment. After merging save and compile. If you are getting errors after save and compile post the screenshot of the errors. If save and compile is successful without any errors, then you can insert an S7 connection. Let me know how it goes! AttachmentDokument1.pdf (222 Downloads) |
2/8/2008 7:55 AM | |
Posts: 3 Rating: (0) |
Hello again, thank you for your answers. I've been trying without succes. In fact I already merged the networks and I defined a S7 connection between the CPU, but when I try to create global data it's not possible to assgin the second CPU to a column. The multiproject has two project called C5 and C6, each one has a MPI network (MPI C5 and MPI C6). I send you some screen shots. I hope it will help. Anyway thank you in advance for the time you spend in this. Have a nice weekend! AttachmentDocumento1.pdf (202 Downloads) |
Follow us on