12/22/2009 1:55 PM | |
Posts: 103 Rating:
|
How are you all , I need to connect my PC to 2 X (CPU 317 2DP) , to make smallMPI network to test something. I have USB adapter <<6ES7972-0CB20-0XA0>> I have made all required steps to implement this network , the pictures in the attachment show that . in PC/PG interface : when I start network detection , SIMATIC detect MPI network but when I make Display accessable node , SIMATIC DetectONE PLC ONLY with MPI=2 another problem : when I was trying to download <<SIMATIC 300(2)>> , SIMATIC MANAGER display error message to me , 'also in the attachment' please help me to solve this problems hint:- I have tried in two cases , PC is only master on the bus selected / not selected I know this is a petty problem but I'm beginner in networking thanks in advance AttachmentMPI.zip (129 Downloads) |
12/22/2009 5:29 PM | |
Posts: 103 Rating:
|
thank IBN-service & ammy ---I connect 2nd CPU & disconnect the 1st CPU this means that SIMATIC 300(2) has something error AttachmentNetwork.zip (108 Downloads) |
12/23/2009 12:19 PM | |
Posts: 8946 Rating:
|
Sorry, I am not egyptian, I am GERMAN. But does that realy matters? A last hint for you: Have a look at SFC67 "X_GET" for MPI - communication also. It is very easy to use but mutch more comfortable than global data. Nice X-mas! |
Last edited by: IBN-Service at: 12/23/2009 12:24 PM |
|
Follow us on