1/3/2019 9:05 PM | |
Posts: 37 Rating: (0) |
hi
how could i mpi as rs-485? and if can use it as rs-485 so whats type of rs-485 will be ? |
1/3/2019 10:12 PM | |
Joined: 9/27/2006 Last visit: 6/1/2024 Posts: 12259 Rating: (2670) |
Hello; The S7-300 and S7-400 PLCs use an integrated MPI port for programming and basic communications with Siemens automation equipment. MPI is based on the RS-485 electrical standard, but it is a dedicated protocol, and the integrated MPI port cannot be used to connect to a 3rd-party equipment for serial commnications. For this you need a serial RS-485 communication processor, either a CP-340 or a CP 341 for the S7-300 CPUs, and you must program the serial data exchanges with the help of configuration software provided when you purchase the CP, or that you can download from this site (use the Search box at the right of this page to locate them). The following link will show you the connections used by the CPs, and links at the bottom of the page will help you see the basics of communication with a CP 340/341. How do you connect the RS485/RS422 interfaces of SIMATIC and SIPLUS modules for serial communication? (Examine figure 3) https://support.industry.siemens.com/cs/ww/en/view/109736665 Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 1/3/2019 10:13:46 PM |
|
This contribution was helpful to1 thankful Users |
1/4/2019 5:32 PM | |
Posts: 37 Rating: (0) |
|
12/15/2019 3:17 PM | |
Joined: 7/9/2016 Last visit: 6/19/2022 Posts: 9 Rating: (1) |
I landed here by searching something like - to use USB to 485 converter to communicate over MPI. AutoGen_912446 might be searching like this! |
Follow us on