7/16/2007 11:46 AM | |
Posts: 672 Rating: (57) |
Hi, The MPI link runs at 187.5K so switch 1 should be off. |
7/17/2007 10:03 AM | |
Joined: 4/26/2007 Last visit: 1/19/2024 Posts: 120 Rating: (8) |
I have MPP connected on BTSS = 1,5MBaud |
7/18/2007 7:34 PM | |
Posts: 17 Rating: (2) |
5,6 ON means address no 6 on the MPI bus. Further down in FB1 call there is address 6 declared as MCP address no. see attached file. Regards, |
7/19/2007 12:20 PM | |
Joined: 4/26/2007 Last visit: 1/19/2024 Posts: 120 Rating: (8) |
My setting for DIP S3 is different, I have DOConCD Sinumerik... 4/2006 See you atachment My setting is OK, becouse if I have 4, 5 ON then panel is present with adress 6 througt MPI diagnstic. I was try other adress and it agree too. AttachmentDIP S3.pdf (244 Downloads) |
7/24/2007 3:15 PM | |
Joined: 4/26/2007 Last visit: 1/19/2024 Posts: 120 Rating: (8) |
How can I insert second communication partner (MPP483) into GD table? See attachment. Tomas |
Follow us on