5/15/2023 1:06 PM | |
Joined: 3/15/2016 Last visit: 1/8/2025 Posts: 6 Rating: (0) |
Hello, I'm on MTP700 and i try to use CreateScreenShoot function but it don't work. My problem is the path of this function. I want create a screenshoot on SD-X51 and on USB-X61. What is the correct syntax for this please ? Thanks ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/16/2023 07:32:09New subject after splitting |
|
5/16/2023 10:12 AM | |
Joined: 1/21/2013 Last visit: 1/21/2025 Posts: 3446 Rating: (543)
|
Hi Aurelien_V2A, On a Unified Comfort Panel, the path to external storage media is "/media/simatic/X51", where X51 can be replaced with any other available interface. For the CreateScreenshot system function, you must specify the full path including the file name and extension, e.g. "/media/simatic/X51/screenshot.jpg". According to the manual ".jpg" and ".jpeg" are possible, but in my test ".png" also worked (tested with V18, Update 1). Kind regards |
Follow us on