10/27/2023 3:44 PM | |
Joined: 12/18/2014 Last visit: 7/5/2024 Posts: 33302 Rating: (4124)
|
I'm sorry, but what is a "SZVTNMV018092"? |
10/28/2023 4:02 PM | |
Joined: 6/11/2019 Last visit: 7/2/2024 Posts: 2204 Rating: (99) |
Hello DMirabella, Yes, something like that is possible with the Logo 5. A program often says more than a thousand words.So here's an example in the appendix: B014 = filling time for small cup B015 = Filling time for large cup B001 = Changeover time to manual filling B009 = Blocking time so that the operator can select the large cup without the time for the small cup starting. Of course you have to adapt the times to the system and your wishes. Greetings Ella_68 (translated with Google) Attachmentautomat_0ba5.zip (347 Downloads) |
11/1/2023 9:28 AM | |
Joined: 6/11/2019 Last visit: 7/2/2024 Posts: 2204 Rating: (99) |
Hello DMirabella, Your old LOGO!Soft should run on its own. At least you can upgrade it to the current version for free. You can find the link here in the forum. I have attached the program as a PDF. Greetings Ella_68 (translated with Google) AttachmentLOGO!Soft Comfort - automat_0ba5.pdf (448 Downloads) |
Follow us on