10/14/2014 6:20 PM | |
Joined: 6/4/2010 Last visit: 11/14/2024 Posts: 72 Rating: (0) |
MicroMan:Thanks for your good support. Already I have seen that document (WinCC V7.0 SP1 MDM - WinCC: Configurations). With that document only I have in Middle of my project. There is no clear description or I'm not able to understand the difference between multi-user system or distributed system. What I should configure for multi-user system and what for distributed system. Both are collasped. Even its very worth document for me. There is no more information about Internal Tags. First I'm going to create new simple project for both multi-user system and distributed system. Hope any one of that system will work for me. Just for a try. |
Regards, |
|
10/15/2014 11:07 AM | |
Joined: 10/3/2010 Last visit: 10/31/2024 Posts: 1563 Rating: (192) |
I have several Multi-Users projects running. Each server has up to 16 clients without own project. Never had a problem with internal tags, not on the servers nor on the clients. |
B r g d s , |
|
10/15/2014 12:27 PM | |
Joined: 6/4/2010 Last visit: 11/14/2024 Posts: 72 Rating: (0) |
@SteBo:Let us share your experiance. Problem identified only on the Server PC. But another two Client PC works well with the Internal Tags and my project looks fine on the Client PC. Any settings or configuration needs to modifiy? Single Server with Two more Clients is enough for me.
@bg2492: Its not a problem. But I have tried both with no success. Currently I have used "Computer Local Update" option for the Internal Tags. |
Last edited by: SelvakumaaR at: 10/15/2014 12:33 PMRegards, |
|
10/17/2014 6:50 AM | |
Joined: 10/3/2010 Last visit: 10/31/2024 Posts: 1563 Rating: (192) |
Hey SelvakumaaR, at this point it's not quite clear what your problem exactly is about. Please provide us with detailed information (what exactly are you trying through VB scripts from SQL???, what behaviour do you notice on the server, on the clients???). Are your scripts made so they can run from server as well as from client?...)? Did you try to run apdiag.exe to monitor possible errors from your scripts?... |
B r g d s , |
|
Follow us on