12/9/2010 8:51 PM | |
Posts: 8 Rating: (0) |
Hallo, I should have to use some kind of multi-VGA cards with a Simatic Rack OC 547B OS Server where is installed Windows Server 2003 and PCS7 7.1. SP1. In the pcs7-readme file it looks that the carda are approved only for Windows XP Pro. But Matrox supplies driver for Windows Server too and, if I understood well, you have already used without problem on server. Isn't it? Thank you in advance for any reply. Regards. Splitted from Multi screen operation - VGA card recommendation. |
Last edited by: O_Moderator at: 12/10/2010 12:59 PMnew subject after splitting |
|
Follow us on