7/17/2023 8:41 AM | |
Joined: 7/19/2022 Last visit: 8/12/2024 Posts: 380 Rating:
|
Hello JorisMullenders, The Comfort panels only support a maximum of 8 connections, so you will not be able to directly connect all these devices to the HMI. Perhaps what you can do is connect 8 devices to the panel and the rest of the devices that are connected and exchanging data with another PLC |
If this Information really helps, you could use the Rate function |
|
Follow us on