4/13/2015 2:48 PM | |
Joined: 6/27/2008 Last visit: 7/6/2021 Posts: 43 Rating:
|
PCS7 V8.1 When compiling CFC I get errors on some CM (imported by AdvES). For example: W: Multiple installation: Instance OT56-DVP.FbkV1 is not installed in OB100. AttachmentAS1_Compile_0413_1419.txt (536 Downloads) |
7/9/2015 9:12 AM | |
Posts: 567 Rating:
|
Hi, can you install the newest Service Pack and Update for CFC and test if the behavior is still the same? But to use CFC V8.1 SP1 Upd 2 you have to update from PCS 7 V8.1 to PCS 7 V8.1 SP1. If it is not possible or the behavior is still the same you shout open a service request. |
8/4/2015 9:58 AM | |
Posts: 21 Rating:
|
Dear all, Did you find a solution for the problem? I am using PCS7 V8.1 SP1 with CFC V8.1 SP1 upd2 and I have the same issue. Regards Gabriel |
11/17/2015 3:31 PM | |
Joined: 5/22/2013 Last visit: 8/28/2024 Posts: 5 Rating:
|
Hi all !!! Try to deactivate "Chart-based insertion" in advanced properites of Charts folder. In my case it work's. |
Follow us on