Industry Online Support
Technical Forum
3/12/2008 9:42 AM | |
Posts: 3 Rating:
|
I think that this manualis what your searches......good luck
AttachmentModsla_e.pdf (1623 Downloads) |
3/12/2008 12:45 PM | |
Joined: 3/11/2008 Last visit: 6/27/2024 Posts: 80 Rating:
|
I want the CP341/441 to be MASTER, and I have the manual for Modbus master https://support.automation.siemens.com/WW/llisapi.dll/1220184?func=ll&objId=1220184&objAction=csView&nodeid0=10805065&ehbid=html%5F76%2Fehb%2F1220184%2Ehtm&nodeid=1219437&lang=en&siteid=cseus&aktprim=0&extranet=standard&viewreg =WW&load=content&csQuery0=6ES7870-1AA00-0YA0&subtype=133300 I think i have figured out how it works for the CP341, if it is true that I don't need to configure anything in NetPro?! But the CP441 is still unclear: - Is it enugh to have only one slave configured in NetPro? Even doughI have 8 slaves? It doesn't seam to be possible to connect more than one slave to one CP441 in NetPro, whichis understandable when PtP network is used. - The data I want to read is at address 41991-42060 (70words), it doesn't seam to be possible to start at a specified address with the SFB13 BRCV block or is it? or must I read from 40000 to 42060? Thank you for all help! |
Last edited by: Kicken at: 12.03.2008 12:49Last edited by: Kicken at: 12.03.2008 12:47Last edited by: Kicken at: 12.03.2008 12:45 |
|
3/14/2008 12:15 PM | |
Posts: 4 Rating:
|
Good luck ! It runs perfectly. Bye AttachmentMODBUS_300_MULTIREQ.zip (1928 Downloads) |
This contribution was helpful to
2 thankful Users |
Follow us on