10/2/2024 2:05 PM | |
Joined: 3/7/2017 Last visit: 11/5/2024 Posts: 15 Rating: (0) |
Hello I tried today the solution with the IP adresse. Reading out the IP adresse and hide/show some elements works fine. However when I try to load the same HMI into 2 different physical screens. They get both the same IP and Profinet name. Can I load the content of an HMI without loading the IP/Profinet name? I tried "extende load to PLC" but it made no difference. I have now 1 HMI in the configuration (TIA portal V19) and I want to load this software into 3 different HMI's with 3 different IP adresses. I am greatfull for any help / advise. Best regards Edit: Hier habe ich einen Eintrag von Murof gefunden der mir zu diesem Thema geholfen hat. |
Last edited by: MaDup at: 10/02/2024 14:24:07 |
|
Follow us on