8/6/2012 6:54 AM | |
Joined: 12/19/2011 Last visit: 2/14/2025 Posts: 36 Rating:
|
Good day! Thank you for your help! We have a PROFIBUS connection diagram shown in the figure. I think the PROFIBUS connection diagram is not correct. Please tell me how to make a connection. AttachmentPROFIBUS.pdf (172 Downloads) |
8/6/2012 8:12 AM | |
Joined: 12/19/2011 Last visit: 2/14/2025 Posts: 36 Rating:
|
Hi For more information on our CNC system. ADI4 module is used to control two analog spindles. Drive SINAMIKS innings. After connecting the Profibus bus NCU - ADI4 - PP72 / 48 and the terminator on the NCU and the PP72 / 48 situation has not changed. (HW gives the same error when trying to view properties ADI4 in online mode) Communication with the modules installed can be seen from the drawings (1 - to view the properties ADI4, 2 - after viewing properties ADI4 in online mode) LEDs on the module ADI4 are green at first and then see the red one Attachmenttemp.ZIP (151 Downloads) |
8/6/2012 9:44 AM | |
Joined: 1/19/2008 Last visit: 2/9/2025 Posts: 992 Rating:
|
Hi, Have you parameterised correctly and set up the equidistant DP cycle. Pee |
Follow us on