12/1/2021 10:21 AM | |
Joined: 3/15/2019 Last visit: 3/11/2024 Posts: 2 Rating: (0) |
Hai Ihave actualy the same Problem, but i use Modbus RTU Does anybody have a idear to solve the problem? I need a way to force the WinCCdriver to force writing with command 16. Thanks in advance ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/01/2021 13:41:04New subject after splitting |
|
12/1/2021 1:42 PM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (171) |
Closed cause question posted twice. The second thread with the subject Want to send the functionskeys from winccruntime to the controller by modbus rtu is published within the conference SIMATIC WinCC flexible. Best regards, |
Follow us on