10/3/2023 9:48 AM | |
Joined: 8/30/2021 Last visit: 10/6/2023 Posts: 6 Rating: (0) |
Oh, it was so simple..? Thank you! Can i get the value from the NAI and output value 4-20mA somehow on the LOGO diplay? |
10/3/2023 9:53 AM | |
Joined: 12/18/2014 Last visit: 5/11/2024 Posts: 33009 Rating: (4079)
|
No, so not. Then must insert a analog amplifier between the NAI and the AQ. |
10/3/2023 10:25 AM | |
Joined: 8/30/2021 Last visit: 10/6/2023 Posts: 6 Rating: (0) |
Can I get the 4-20mA value from the AQ on the display? Tried with the Analog amplifier, but no luck... |
10/3/2023 10:41 AM | |
Joined: 12/18/2014 Last visit: 5/11/2024 Posts: 33009 Rating: (4079)
|
See attachment ...
AttachmentNAI_to_AQ_0BA8.Standard.zip (328 Downloads) |
10/4/2023 5:19 AM | |
Joined: 12/18/2014 Last visit: 5/11/2024 Posts: 33009 Rating: (4079)
|
@DeaWillfor, no statement to my last post? |
Follow us on