7/23/2019 5:21 PM | |
Joined: 8/23/2018 Last visit: 11/19/2020 Posts: 9 Rating:
|
How to increase the interval? Attached is the diagnostic buffer txt file. The issue at my production line is sometimes my input module suddenly low on 24DC even though I have increased the value to 25VDC. Already replace my Profibus socket and add RS485 repeater to boost the signal. Need help
AttachmentDiagnose.txt (191 Downloads) |
Follow us on