Industry Online Support
Technical Forum
12/13/2007 12:55 PM | |
Posts: 1 Rating: (0) |
Hi! I'm generaly working with PLC's and hardware and I'm new at SCADA, maybe someone more experienced can help me with my issue.. I have transfered WinCC project from one PC to another, and now have problem with scripting runtime actions (*.pas files). In brief - script is collecting every hour data from SIMATIC PLC, places it in temporary placeholders - WinCC internal tag's, and on a daily baisis calculates average, min and max values, placing them also in WinCC internal tag's. Then thouse values are used to generate and print report. But instead of calculated values I get zeros. It seems that script can't collect or store data, or it can't do calculations. And in the WinCC_Sys.log I get every day an error "SCRIPT,ExecuteError in Action @<address>". Executed actions are attached in .zip archive. Maybe, you can help me in identifying most obvious causes? Or some method to debug scripts without interfering with running project? Thank You in advance! With best regards, Dmitrijs Kilups AttachmentPAS.zip (108 Downloads) |
12/14/2007 12:55 PM | |
Posts: 1776 Rating: (95)
|
Hi, for diagnostic see the FAQ http://support.automation.siemens.com/WW/view/en/22892165 April |
Follow us on