11/14/2018 5:15 PM | |
Joined: 12/27/2011 Last visit: 7/14/2023 Posts: 1 Rating:
|
hi, i am converting program S5 95u to S7, please i need some help me to identify the logic below: NAME: FORM57 A DB 50 UN M 13.4 BEB L KY 124,10 T MW 220 L KY 60,10 T MW 224 L KF +50 T MB 226 SPA FB 73 NAME: DB->DB SOUR: MW 220 DEST: MW 224 LONG: MB 226 L KY 126,10 T MW 220 L KY 61,10 T MW 224 L KF +50 T MB 226 SPA FB 73 NAME: DB->DB SOUR: MW 220 DEST: MW 224 LONG: MB 226 BE FB 73 is: NAME: DB->DB BEZ : SOUR EW BEZ : DEST EW BEZ : LONG EBY L =LONG SLW 1 T MB 206 L =SOUR T MW 200 L MB 200 SLW 1 L KH 7E00 +F LIR 0 L MB 201 SLW 1 +F L MB 206 +F L KB 1 -F T MW 202 L =DEST T MW 200 L MB 200 SLW 1 L KH 7E00 +F LIR 0 L MB 201 SLW 1 +F L MB 206 +F L KB 1 -F T MW 204 L MW 202 L MW 204 TNB 100 BE thanks in advance ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/15/2018 9:38:53 AMNew subject after splitting |
|
11/15/2018 10:06 AM | |
Joined: 7/9/2015 Last visit: 9/20/2023 Posts: 3539 Rating:
|
Hi, please check the following Manual: SIMATIC STEP 7 V5.5 From S5 to S7Regards, Towome
|
If my post was useful, please rate me - thank you! |
|
Follow us on