5/17/2024 11:44 AM | |
Joined: 5/12/2023 Last visit: 5/20/2024 Posts: 4 Rating:
|
I want to download the Setup of PCS 7 V8.1 SP1. From where will i get the setup? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/17/2024 12:00:42New subject after splitting |
|
5/29/2024 6:38 PM | |
Joined: 3/14/2008 Last visit: 6/18/2024 Posts: 2070 Rating:
|
Hi, In order to use discontinued products like PCS7 V8.1, you need a legacy contract which allows you to get updates/licenses and support. See link below. Base versions aren't listed as downloads on the SiePortal, only updates. For PCS7 V8.x, downloads and manuals are not possible anymore from the website as the product is discontinued. |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on