5/8/2008 7:21 AM | |
Posts: 56 Rating: (1) |
I am new in this fourm.I have need of GSD file for the below mentioned siemens order no 6ES7 313-6CF03-0AB0 Please help me in this regards |
5/8/2008 7:33 AM | |
Joined: 9/27/2006 Last visit: 8/12/2024 Posts: 12276 Rating: (2680) |
Hello ttt singh; You willbe able to downloadall gsd files for S7 CPUs (-2DP) on the fiollowing page from Product Support (see the link at the top of the forum page): http://support.automation.siemens.com/WW/view/en/113652 Hope this helps, Daniel Chartier |
5/8/2008 11:08 AM | |
Joined: 3/21/2006 Last visit: 7/26/2024 Posts: 10228 Rating: (1181) |
Hi Unzip attachment and in HWConfiguration-Open OPTIONS - Edit Catalog Profile - and IMPORT this CPU300 Profile. After that you can chose this profile in catalog and... Regards Umencho AttachmentCPU300.zip (815 Downloads) |
5/8/2008 2:47 PM | |
Joined: 3/21/2006 Last visit: 7/26/2024 Posts: 10228 Rating: (1181) |
Hi When imported this hardware catalog you will see one folder with name:6ES7 313-6CF03-0AB0. On the other side will see two firmware version of this CPU - v2.0 and v2.6. And then when go in hardware catalog and chose this will see this folder with +. Click under folder and must see two version of this CPU (firmware). See attachment. regards Umencho Attachmentplc.zip (654 Downloads) |
Follow us on