8/13/2023 9:53 AM | |
Joined: 7/5/2023 Last visit: 8/13/2023 Posts: 1 Rating: (0) |
Hi, can you please write a program to scale an RTD, thermocouple and pressure transmitter between 0 and 14 bar ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 08/14/2023 11:18:46New subject after splitting |
|
8/23/2023 6:11 PM | |
Joined: 6/20/2017 Last visit: 7/10/2024 Posts: 377 Rating: (36) |
And, the next query will be the entire machine program? |
Gustavo Antonio Banchetti Brucatori. |
|
8/24/2023 5:42 AM | |
Joined: 6/19/2019 Last visit: 7/10/2024 Posts: 697 Rating: (73) |
I think you need use norm_x then scale_x functions and you will have your correct value Let's see any video on youtube how to do that, or I can put one random link from youtube link HERE |
Last edited by: The Helping Hand at: 08/29/2023 07:40:13Video embedded. |
|
Follow us on