7/1/2023 10:20 AM | |
Joined: 7/1/2023 Last visit: 7/19/2023 Posts: 1 Rating: (0) |
Hi I Need servo motor slection for fiber laser cutting machine purpess. machine Bed size 6500mm/2500mm Gantery total Weight 530 kg Y&V X axis total weight 150 kg Z axis total weight 30 kg Helical gear with moduel 2 ratio 7 pinion OD 71.9 pls sugesst Motor size, ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 07/03/2023 09:02:10New subject after splitting |
|
7/4/2023 8:59 AM | |
Joined: 10/11/2006 Last visit: 7/26/2024 Posts: 5880 Rating: (799)
|
Hello, you can use the engineering tool SIZER / Tia Selection Tool to determine the motor according to the load. Tia Selection Tool (desktop version): |
With best regards, |
|
Follow us on