2/6/2018 12:56 PM | |
Posts: 6 Rating: (0) |
Morning; I am working on the modeling of an asynchronous motor , and to do so I need some parameters related to the motor such as : Rotor resistance , Stator resistance Inductances ( of the rotor , of the stator )and mutuelle inducance ) It's urgent , thank you for being helpful. Greetings B.S ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 2/6/2018 1:44:21 PMNew subject after splitting |
|
2/6/2018 8:17 PM | |
Joined: 5/22/2012 Last visit: 3/24/2022 Posts: 895 Rating: (67) |
Hello following you will find the definition of the SINAMICS motorparameters: https://support.industry.siemens.com/cs/ww/en/view/79690594 The motorparameter themselves for the listmotors you can see in the STARTER / STARTDRIVE software where you can choose a motor and the motorparameters would be preseted by the software. Best regards Zako |
This contribution was helpful to1 thankful Users |
Follow us on