2/17/2022 9:04 PM | |
Joined: 4/29/2021 Last visit: 2/16/2024 Posts: 5 Rating: (0) |
Hello, I need the configuration of the transfer cable of the Protool for a S7-633 DP. Does anyone have the cable configuration and which port to use on the PLC C7-633 DP? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 02/18/2022 10:18:56New subject after splitting |
|
2/18/2022 8:41 AM | |
Joined: 4/24/2006 Last visit: 5/8/2024 Posts: 8638 Rating: (1151)
|
Hello, To connect to PLC, you need MPI cable (Port X3) (Pinout is straight cable, you need pin 3, 5 and 8) To connect to Operator panel, you need the cable 6XV1440-2KH32. (Port X2) Here you find a pinout: What connecting cables are there for connections between the operating units and the different controllers? Here is a link to manual: C7-633 / C7-634 Control Systems Best regards, Wizard |