2/11/2019 12:58 PM | |
Posts: 3 Rating:
|
hi there guys my new PC doesn't have a PCMCIA card slot and I sit with the CP5512 card adapter please inform or advise me on what card reader is available for me to use and where I can get hold of this reader ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 2/12/2019 9:38:17 AMNew subject after splitting |
|
2/11/2019 1:12 PM | |
Joined: 5/12/2006 Last visit: 4/15/2025 Posts: 22613 Rating:
|
Hello, which Card slot you have on the new Laptop? CP5512 is not compatible with any 64bit Operation system! Only for Win7 32bit a driver is available, not for Windows10.
Christoph |
2/11/2019 3:07 PM | |
Posts: 3 Rating:
|
Hi Christo My current OS is windows 10 but that is okay for all the newer stuff. Im also running a Virtual machine with windows 7 and XP for the older stuff and that is where I need the CP5512 adapter ,currently on my laptop I do have either net ,SD,USB ports |
2/20/2019 2:03 PM | |
Joined: 8/3/2009 Last visit: 4/14/2025 Posts: 15280 Rating:
|
Hello We had also a similar situation a few years ago. We have changed all DP/MPI Adapters to CP5711 (USB CP) and It works without problems and also a lot easier in VM Wares. We tried in the beginning also with Adapters and so on but this works not compleatly good. Bye Murof |
If this Information really helps, you could use the Rate function |
|
2/4/2021 7:25 PM | |
Joined: 9/8/2013 Last visit: 10/15/2024 Posts: 1 Rating:
|
CP5512 maybe is not compatible with x64 but it can work with Windows 10 x64 and TIA. |
Last edited by: PX1 at: 02/04/2021 19:26:49 |
|
We are working on a new user interface with better overview and more relevance.
Follow us on