4/9/2018 5:21 AM | |
Posts: 107 Rating: (0) |
Hi all. Support me please with AS (of PCS7 v8.1) I need to change setting of CP443-1 in properties Time-of-Day synch. tab. in the SIMATIC Mode from From station to LAN to Automatic then when I download it will it stop CPU-410 ? Found in the manual only for replacement but for this small change no. thanks IT_Service ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 4/9/2018 3:00:35 PMNew subject after splitting |
|
4/9/2018 7:00 AM | |
Joined: 9/9/2015 Last visit: 9/4/2024 Posts: 727 Rating: (278) |
Hi IT Service, CPU410-5H could do a download in run. If the redundancy of the entire network is okay, it should not be stopped. Try press download in run, the system will tell you whether there is a redundancy issue or not. Hope it helps. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
4/9/2018 5:10 PM | |
Posts: 107 Rating: (0) |
Thanks for detailed answer.. Let me check. Thanks IT_Service |
5/9/2018 8:51 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (171) |
New question published by IT service is split to a separate thread with the subject In the real CPU not transferring to MD50 . Best regards |
Follow us on