7/5/2021 5:58 PM | |
Joined: 3/8/2016 Last visit: 2/18/2022 Posts: 1 Rating:
|
Hello, I have been trying to assign the command directly from the IOP for 5 days using macro 47 but I have not been successful. Could you help me with the parameters that I must put in the custom hand mode IOP so that it works correctly. I have a 0-10 bar pressure sensor. Which already connects to the analog input A01. I require the drive to keep the PID regulator at a 4 bar setpoint. And it is precisely that I do not know where to place this command directly from IOP-2. I will greatly appreciate your support. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 07/06/2021 08:08:59Edited text for better reading. Last edited by: Jen_Moderator at: 07/06/2021 08:09:47New subject after splitting |
|
Follow us on